FB#.RESREFPHASE
Description
This parameter sets the electrical degrees of phase lag in the resolver.
See the motor resolver datasheet for the value for this parameter.
Context
See Feedback Devices.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
electrical degrees |
Range |
-180 to 180° |
Default Value |
-2° |
Data Type |
Float |
See Also |
N/A |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDOPDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | FB1.RESREFPHASE | 0x3500 | 0x5 | UDINT | - | - | RW | False |
FB2.RESREFPHASE | 0x3501 | 0x5 | UDINT | - | - | RW | False | |
FB3.RESREFPHASE | 0x3502 | 0x5 | UDINT | - | - | RW | False | |
FB4.RESREFPHASE | 0x3503 | 0x5 | UDINT | - | - | RW | False | |
FB5.RESREFPHASE | 0x3504 | 0x5 | UDINT | - | - | RW | False |